cancel
Showing results for 
Search instead for 
Did you mean: 

[BUG][V2.20] -noreconnect doesnt work on Windows

dnugent
Associate II

I recently tried to use -noreconnect via the cli on windows and it still attempted to reconnect.

I was connected via UART and programming option bytes. 

Here was the command I used:

& "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=COM14 br=115200 -noreconnect -ob ndbank=0x0

I see that there was fix put in for linux. Im wondering if the same bug exists on Windows.

Thanks,

Daniel

 

1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee

Hello All,

Thank you for posting and for all the details you provided.

I escalated this issue to the relevant team (through internal ticket number 218005) to take a closer look at the problem.

(PS: ticket number 218005 is an internal tracking number and is not accessible or usable by customers).

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

8 REPLIES 8
uh_oh
Associate

I encountered the same issue with -noreconnect still attempting to reconnect in v2.20 on Linux.

I am programming option bytes on the U575 via USB.

The command I ran and its output are included as an attachment.

fma
Associate II

I'm having the same issue when using API v2.20 on Windows. 

dnugent
Associate II

Thanks for the confirmation and work arounds.

I assumed posting here was filing the bug with ST. Is there a different place for that?

 

Daniel

Imen.D
ST Employee

Hello All,

Thank you for posting and for all the details you provided.

I escalated this issue to the relevant team (through internal ticket number 218005) to take a closer look at the problem.

(PS: ticket number 218005 is an internal tracking number and is not accessible or usable by customers).

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee

Hi All,

We confirm this issue. 

Thank you again for highlighting this issue. Your feedback has been very helpful in raising the ticket along to our development team for fix.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
atibelettronica
Associate

I'm using STM32CubeProgrammer API but I don't find the command to no reconnect to device after OB programming. Could you list the procedure to do that? Thanks

cheeric
Associate

Just like to echo this thread and add that the -noreconnect command still doesn't seem work for STM32CubeProgrammer v2.21.0 on Windows 11

Looking forward to a fixed release.

Thanks,
Eric

Hello all,

Issue is fixed in the latest STM32CubeProgrammer release available here.

Aziz


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.