STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32L051R8 Program Issue with Cube Programmer

I am working with the L051 chip and having issues with the CubeProgrammer Download..History:   we work with many of the STM32 chips.....and have for years, so well versed in this ...so this is an issue that we have not seen using any of the Tools... ...

CTerr.1 by Associate II
  • 3263 Views
  • 6 replies
  • 0 kudos

Connection issue

"My STM32 is locked out of its program. How can I unlock it? I need to continue learning to use it, even though I've just started." STMicroelectronics ST-LINK GDB server. Version 7.5.0Copyright (c) 2023, STMicroelectronics. All rights reserved. Start...

bbb by Associate
  • 1395 Views
  • 2 replies
  • 2 kudos

Resolved! NUCLEO-U575ZI-Q board "Error: No STM32 target found"

Using the STM32CubeProgramer (v2.16 from a Windows 11 laptop) with my NUCLEO-U575ZI-Q board has, from this morning, resulted in only the response:UR connection mode is defined with the HWrst reset modeST-LINK SN : 003E004C3532510F31333430ST-LINK FW :...

Cube Prog API Error write memory

I am using C# to wrap the native CubeProgrammer_API.dll to call download file. I am running on x64 machine.When I compile the C# code as x86 and use the x86 version of the DLLs from the SDK, the download went fine.However if I compile the same code a...

zhoupn by Associate
  • 1156 Views
  • 1 replies
  • 0 kudos

STM32Cubeprogrammer no target found

I recently got into dual core mcu (STM32H755ZI) programming and made the common mistake of not configuring the cores correctly and now the board would not connect (I used the STM32CubeProgrammer to flash one of the two .hex files into the device memo...

ZiroKun_1-1713944659714.png ZiroKun_2-1713944752879.png
ZiroKun by Associate II
  • 1217 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeProgrammer Option bytes settings

I am using the latest version of the STM32CubeProgrammer (v2.16.0) and am connected to a STM32F405RGT6 via an ST-LINK/V2.The problem is finding the nBoot0 and nBoot1 settings under the Option bytes tab in the software. Does anyone know where I can fi...

mathieusteketee_0-1713879071922.png

Can't write option bytes with stm32cubeprogrammer

Is there any option to write option bytes to control the boot option for STM32G070 from uart after the first upload or any solution to change the option bytes from stm32cubeprogrammer?I can't change the boot config from option bytes using the stm32cu...

0693W00000JPQuLQAX.png
VPurb.1 by Associate
  • 2577 Views
  • 2 replies
  • 0 kudos

Resolved! STM Cube Programmer Server Connection error

When I open the Cube Programmer (2.14) I'm greeted by a Connection error message:The server connection is not established.The network connection is required to download updates.Please check your proxy settings. I'm not behind a proxy and tried variou...