cancel
Showing results for 
Search instead for 
Did you mean: 

Why in CubeMX the sum of the two parameters must be be 32?

BJX
Associate II

New question split from this thread.

Hello,

Thank you for your response. I have double-checked and found that the 6.10 version also cannot be configured in this way. I will adopt the single-line mode on the next hardware version.

However, there is still a question regarding the configuration of can in version 6.16. Why must the sum of the two parameters in the following figure be 32? Otherwise, there will be a warning. In version 6.13, this issue does not exist.

BJX_0-1764905583381.png

The attachment contains the relevant IOC files.

Love me in the eye.
1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @BJX 

The CubeMX should allow (TX Buffers Nbr + TX FIFO Queue Elmts Nbr ≤ 32 ) instead of ((TX Buffer Nbr + TX Fifo Queue Elmts Nbr) == 32

A ticket (ID: 222211) has been escalated to the development team to address and correct this behavior.

 

Regarding this point :"Both TX and RX pins must be assigned simultaneously; otherwise, the UART peripheral cannot be enabled." :  MX 6.10.0 and MX 6.16.0 are behaving the same way , in Asynchronous mode  both pins are reserved.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.