cancel
Showing results for 
Search instead for 
Did you mean: 

Wave generation of particular frequency.

LACTIC
Associate II

By using timer I want to generate a wave of 27Mhz frequency. Present time I can generate only 13.48khz frequency wave. My timer settings are below please tell me how can I generate it.

static void MX_TIM2_Init(void)

{

 TIM_ClockConfigTypeDef sClockSourceConfig;

 TIM_MasterConfigTypeDef sMasterConfig;

 TIM_OC_InitTypeDef sConfigOC;

 htim2.Instance = TIM2;

 htim2.Init.Prescaler =27;

 htim2.Init.CounterMode = TIM_COUNTERMODE_UP;

 htim2.Init.Period = 1000;

 htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV4;

 htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;

 if (HAL_TIM_Base_Init(&htim2) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;

 if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 if (HAL_TIM_OC_Init(&htim2) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

 if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 sConfigOC.OCMode = TIM_OCMODE_TOGGLE;

 sConfigOC.Pulse = 250;

 sConfigOC.OCPolarity = TIM_OCPOLARITY_HIGH;

 sConfigOC.OCFastMode = TIM_OCFAST_DISABLE;

 if (HAL_TIM_OC_ConfigChannel(&htim2, &sConfigOC, TIM_CHANNEL_4) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

 HAL_TIM_MspPostInit(&htim2);

}

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
LACTIC
Associate II

Please suggest how can in  generate a wave of 27Mhz frequency. Timer settings are mentioned in above massage.

RomainR.
ST Employee

Hello,

Can you please detail which STM32 device, and APB Clock frequency you have set ?

Change htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

Not TIM_CLOCKDIVISION_DIV4;

27MHz / 4 = 6.75 which is the half of 13.5MHz you measure.

BR

rrom

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello,

Ok. I will cange it.

I am using STM32f207ZGT6.

Sorry it is "change" not cange.

S.Ma
Principal

if you core runs at 108 MHz and say this goes direct to feed timer clock, your timer can count only up to 4 as period.

Then set the toggle point to 2 and you get 50% duty cycle at 27MHz.

0123012301230123

__--__--__--__--__

Or more fun, if you use a SPI as master with DMA cyclical to a dummy buffer, its maximum clock SCK will run at SYSCLK/2 = 54 MHz (if fast SPI, STM32 family dependent)

S.Ma
Principal

Also look at MCU output pin, which can output internal clock with simple prescale factor. Simple cheap, keeps more complex peripherals available.

==> Reference Manual

System clock settings :-

void SystemClock_Config(void)

{

 RCC_OscInitTypeDef RCC_OscInitStruct;

 RCC_ClkInitTypeDef RCC_ClkInitStruct;

  /**Initializes the CPU, AHB and APB busses clocks 

  */

 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;

 RCC_OscInitStruct.HSEState = RCC_HSE_ON;

 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;

 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;

 RCC_OscInitStruct.PLL.PLLM = 4;

 RCC_OscInitStruct.PLL.PLLN = 216;

 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;

 RCC_OscInitStruct.PLL.PLLQ = 4;

 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

  /**Initializes the CPU, AHB and APB busses clocks 

  */

 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

               |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;

 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV8;

 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)

 {

  _Error_Handler(__FILE__, __LINE__);

 }

  /**Configure the Systick interrupt time 

  */

 HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);

  /**Configure the Systick 

  */

 HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

 /* SysTick_IRQn interrupt configuration */

 HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}

cubmex clock config window.