cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F407VGTx / CDC / Error Driver

CC_ROB
Associate II

Hello,

I test the CDC with my STM32F407VgTx in an up-to-date environment:

 Windows 10 / STM32CubeMx v5.20 / SW4STM32 / System WorkBench for STM32/ST-LINK V2

The VCP v 1.50 driver for windows 10 has been installed normally and declared active.

The source of the CDC program used is:

\ STM32Cube_FW_F4_V1.24.0 \ STM32Cube_FW_F4_V1.24.0 \ Middleware \ ST \ STM32_USB_Device_Library \ Class \ CDC

When running the program, when init the USB, I get Windows Error 43.

 Unknown USB Device (descriptor request failure).

Can you help me solve this problem?

In advance thank you

Robert

This discussion is locked. Please start a new topic to ask your question.
29 REPLIES 29

Hello Christian,

The retrogradation of the 6 files did not solve the problem.

My anomaly has causes different from those you hads

Thanks

Robert

CC_ROB
Associate II

VCP CLEANFLIGT

CDC OK

Pavel A.
Super User

The picture you've posted 2 days ago shows a problem with USB clock. Have you resolved it? Does the board have external oscillator for HSE?

-- pa

CC_ROB
Associate II

Hello,

Sorry to have mixed HSE / HSI in the text 2 days ago.

My card has an external crystal of 26 Mhz / HSE

I'm doing my tests in this extern crystal config

I had been told that the CDC was working in 16 Mhz / HSI but when I saw that there were clock config problems I did not try.

That said if there was a solution to work with the USB without extern crystal outside I would be a taker.

Rob

CC_ROB
Associate II

Hello,

Addition LED2 control by PE0

Libs version 1.24.1

New ioc file attached.

Pavel A.
Super User

>  if there was a solution to work with the USB without extern crystal outside I would be a taker.

Some MCUs with device-only controller (F072 for example) can derive the USB clock from host, using SOF.

They can work without external crystal. I don't know whether OTG can do this, even in device mode.

-- pa

Hello,

After having done, with the community that was interested in this problem, all the investigations that seemed interesting to us,

the problem I described is not solved .

My last investigations with DBG_Trace (present in the project) allowed me to see that the interrupts resulting from a request of the driver (OTG_FS_IRQHandler > HAL_PCD_IRQHandler (& hpcd_USB_OTG_FS) are active and processed but I could not delve deeper to locate the problem ...

The VCP driver for Windows10 does not receive (in 3ms I believe) correct information in descriptor (for him) and reports it in the program manager of Windows 10.

The same thing happens under Windows 7 professionnal.

It should be noted that this driver works without error with several other VCP applications found on the net that I tested on my DIYMORE card.

We can think that the problem lies in the libraries of version 1.24 / 1.24.1 or in the projet generated by CubeMX .

I am attaching my complete project.

Hoping to have a solution as soon as possible ....

At advance thanks.

Regards.

Robert

Harry McKee
Associate II

I think I'm having the same problem (but with an L4 and F7 board). I've got debug output on another thread: https://community.st.com/s/question/0D50X0000Ap1YIzSQM/do-the-virtual-com-port-drivers-work-with-windows-7

Please take a look and see if this is similar to your issue.

When I run it on a Windows 7 system, I get the USB error 10. Window Server 2012 systems shows USB error 43.

The issue I'm seeing has been fixed. It was an unaligned memory access in USB_WritePacket.

Hello,

Thank you for your information.

My error code is different from yours : 43 in Windows 7 and 10 .

I still modified USB_Write Packet (...) but the problem has not been solved.

CC_ROB
Associate II

Hello,

Same problem with last version (5.2.1) of STM32CubeMX.

Sorry.

Robert.