cancel
Showing results for 
Search instead for 
Did you mean: 

MX_TouchGFX_PreOSInit() called before I can init my external (QSPI) Flash

MHoll.2
Senior III

The STM32CubeMX generated main.c has the function MX_TouchGFX_PreOSInit() called directly after the MX_xxx_Init() functions, before I can insert my External Flash Initialisation (in /* USER CODE BEGIN 2 */).

This prevents the use of the External Flash for the TextFlashSection defined by TouchGFX.

It would be better to call MX_TouchGFX_PreOSInit() immediatly before MX_xxx_Init() (in my case  MX_ThreadX_Init()).

1 ACCEPTED SOLUTION

Accepted Solutions

Hello @MHoll.2 

As my understanding you can initialize the External flash inside the MX_OCTOSPI1_Init() (/* USER CODE BEGIN OCTOSPI1_Init 2 */). This will ensure that the external flash is initialized before the call of MX_TouchGFX_init.

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4
Souhaib MAZHOUD
ST Employee

Hello @MHoll.2 

What MCU are you using? Or could you provide your IOC in order to investigate further the issue.

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Souhaib,

I'm using the STM32H725IEK.

Attached a small example ioc file that generates

/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{

  /* USER CODE BEGIN 1 */

  /* USER CODE END 1 */

  /* MPU Configuration--------------------------------------------------------*/
  MPU_Config();

  /* MCU Configuration--------------------------------------------------------*/

  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();

  /* USER CODE BEGIN Init */

  /* USER CODE END Init */

  /* Configure the system clock */
  SystemClock_Config();

  /* USER CODE BEGIN SysInit */

  /* USER CODE END SysInit */

  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_OCTOSPI1_Init();
  /* Call PreOsInit function */
  MX_TouchGFX_PreOSInit();
  /* USER CODE BEGIN 2 */

  /* USER CODE END 2 */

  MX_ThreadX_Init();

  /* We should never get here as control is now taken by the scheduler */

  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */

    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

  I'm using STMCubeIDE 1.18.1, beause of  this problem:  https://community.st.com/t5/stm32cubeide-mcus/stm32cubeide-1-19-0-problem-migrating-octospi2-stm32h730-from-1/td-p/819983

 

Martin

Hello @MHoll.2 

As my understanding you can initialize the External flash inside the MX_OCTOSPI1_Init() (/* USER CODE BEGIN OCTOSPI1_Init 2 */). This will ensure that the external flash is initialized before the call of MX_TouchGFX_init.

BR, Souhaib

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hi Soubaib,

You are right, I whould like to have all my code in main(), but if this is the only solution I will put my flash init code inside MX_OCTOSPI1().

Best regards

Martin