2024-08-30 05:01 AM
Hello dear community,
I'm using a STM32U5A9J-DK.
I want to start in CubeMX a project based on this board, X-CUBE-TOUCHGFX and X-CUBE-GNSS softwares.
However, CubeMX warns me (in the "Software Packs Component Selector") that theses are incompatibles between them.
For example, if I choose X-CUBE-GNSS first then try to choose TouchGFX, it tells "This component cannot be selected: this application cannot be selected while the application from pack STMicrolectronics.X-CUBE-GNSS1.6.0.0 is selected":
and vice versa.
I guess that is because the touch screen use PI6 (DSI_BL_CTRL) pin that can be used as reset pin or wake up pin for GNSS: is this correct ?
Is there a way to "force" or bypass this recommendation ?
Thanks a lot in advance for your help