cancel
Showing results for 
Search instead for 
Did you mean: 

can't set compiler option in top level CMakeList

dvescovi
Senior

Not sure if this belongs in CubeMX or STM32 code for VS.

I have a CMAKE project generated from CubeMX.

When I build within VS Code IDE with the STM32 Extension I get several nocent warnings I would like to eliminate.

Some of these are deep in the HAL and/or the generated code produced by CubeMX.

ex:

warning: declaration of 'hrtc' shadows a global declaration
warning: cast increases required alignment of target type [-Wcast-align]
etc.
I tried several modifications to my top level CMakeLists.txt suggested by AI to suppress these warnings but NONE work.
I know this line:
include("cmake/gcc-arm-none-eabi.cmake")
brings in all the gcc compile options but I don't want to modify this file as it gets regenerated every time I do a CubeMX "GENERATE CODE"
 
Things I have tried are:
set(CMAKE_C_FLAGS "${CMAKE_C_FLAGS} -Wno-shadow")
target_compile_options(my_target PRIVATE -Wno-shadow)
set(MCU_GCC_FLAGS "${MCU_GCC_FLAGS} -Wno-shadow")
add_compile_options(${MCU_GCC_FLAGS})
add_compile_options(-Wno-shadow)
set(CMAKE_C_FLAGS_INIT "-Wno-shadow") include("cmake/gcc-arm-none-eabi.cmake")
add_compile_options("$<$<COMPILE_LANGUAGE:C>:-Wno-shadow>")
set_property(DIRECTORY ${CMAKE_CURRENT_SOURCE_DIR} APPEND PROPERTY COMPILE_OPTIONS -Wno-shadow)
 
NONE of these work.
 
HELP
 

 
 
 
 
 
 
 
1 REPLY 1
Ghofrane GSOURI
ST Employee

Hello @dvescovi 

First let me thank you for posting.

If you could share your IOC file, I’d be happy to review it and provide suggestions or assistance where needed.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.