STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1575 Views
  • 0 replies
  • 2 kudos

SWV not working with STM32CubeMX on TrueStudio

I'm working with a Stm32 Nucleo F429Zi board and I am having trouble getting the SWV working when debugging. When I created a blank new project and went through the Atollic tutorial to redirect printf() to go to _write() and eventually ITM_SendChar()...

DMeye by Associate II
  • 849 Views
  • 0 replies
  • 1 kudos

Resolved! Problem with project converted from CubeMX 4.25.0 to 4.26.1. ADC configuration Scan Conversion Mode broken.

STM32F767 project, converted from 4.25.0 to 4.26.1, now it has an error in the ADC1, 2, and 3 configuration where the Scan Conversion Mode is set to Enabled. This value is apparently bogus and I must pick a new value from the drop down list that only...

Bug Report - USB - STM32F446 / STM32CubeMX

Posted on December 22, 2017 at 14:44Dear ST,First is there any publicly available Bug report site?Found with SMT32CubeMX Version 4.23.0and using the latest firmware package for stm32f4 (1.18.0)USB Custom HID Device: STM32CubeMX Parameter Setting: U...

CubeMX incorrect systick using TIM6

Posted on May 24, 2017 at 10:49CubeMX (latest version: 4.21.0) advises NOT to use the 'systick' clock has HAL systick source when FreeRTOS is used (a message box pops up when generating code). So I switched to TIM6.When doing this the generated code...

andrea2 by Associate
  • 2606 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CUbeMX : RTC options for STM32F1

Posted on November 20, 2017 at 16:58On our custom board we don't use RTC clock for time or date.But I need to activate RTC to use Backup registers, and we use GPIOC PIN13 in mode OUTPUT_PP for leds.With STM32CUbeMX 4.23.0 and STM32CubeF1 package 1.6...

Could not able to work with DMA

I would like to transfer the data coming to ADC to DMA and average the signals after 15 seconds. I could able to read the values from ADC BUT here are my problems. I am using industrial acceleromoeter while reading adc values i could able to see them...

Apill by Senior
  • 1263 Views
  • 1 replies
  • 0 kudos

cubemx stm32 feature request: support custom VECT_TAB_OFFSET

Posted on February 06, 2016 at 23:01Hello, while dealing with custom bootloader we have to switch application to certain offset address. Thus we have to move the address of the vector table. While HSE values are supported to be customized vector tab...

taraben by Senior
  • 2278 Views
  • 8 replies
  • 0 kudos