STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1722 Views
  • 0 replies
  • 2 kudos

Header files missing when building the project

Hi,I have stm3241g-eval board and I created very simple project with it using CubeMX, the latest version. Just USB HS and FreeRTOS enabled and created code. Then Started TrueStudio, also latest version, and opened project from file system.Now when I ...

valtteri by Associate II
  • 2557 Views
  • 2 replies
  • 0 kudos

No GPIO on Nucleo-G071RB Pinout and Configuration

STM32CubeMX Board Selector does NOT show NUCLEO-G071RB, so I select MCU Selector and search STM32G071RB. STM32CubeMX shows NUCLEO-G071RB on Board Colum.I click NUCLEO-G071RB and I Start Project, Initializing all peripherals with their default Mode YE...

NR-A Comm by Associate II
  • 3039 Views
  • 4 replies
  • 0 kudos

New interface

New interface of CubeMX is fancy, but how am I supposed to use it on the screen with resolution lower than full hd? The idea that all the information should be on the screen simultaneously is so useful on small resolution screen. Is there a way to sw...

VArte by Associate
  • 2351 Views
  • 5 replies
  • 0 kudos

Code generation

After generating code for STM32F031K6 in MDK v5 Cube sets target as STM32F031K6Tx, but in CMSIS pack it is just STM32F031K6Similar problem is with 334 seriesYou have to change the target every time you regenerate code. Previously there was no problem...

VArte by Associate
  • 712 Views
  • 0 replies
  • 0 kudos

Problem with STM32CubeMX install on Mac

I'm running MacOS Mojave 10.14.3, trying to install STMcubeMX 5.1.0. I had to install Java 6 legacy and also JRE 8 build 201. When I try to install from the "en" directory created by the STM32cubeMX download using a terminal, here's what I get: (t...

WSank by Associate II
  • 3292 Views
  • 6 replies
  • 0 kudos

STM32CubeMX project generation have problem BUG on samba

​Hello.I work on Windows on a network drive.The file server is samba which, by default, for files whose name starts with a dot, gives the hidden attribute.After generating the TrueStudio project, the .project and .cproject files are thus given a hidd...

SKape by Associate II
  • 895 Views
  • 0 replies
  • 0 kudos

STM32CubeMX generated folders empty

When i generate a project with STM32CubeMx 5.1.0, codes are comes up but the folder below is always empty. Why? I was using the previous version before.\Drivers\CMSIS\Device\ST\STM32F4xx\Source\Templates

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.