STM32CubeMX (MCUs)

Ask questions on STM32CubeMX. Discuss code generation and configuration challenges, among other topics.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX 6.17.0 released

We are pleased to announce that version 6.17.0 of STM32CubeMX is available. What is new in 6.17.0: Added support for new microcontrollers across the STM32WBA, STM32H5, and STM32U3 seriesAdded support for new boards: NUCLEO-WBA25CE1, NUCLEO-H5E5ZJ, ST...

Aimen1 by ST Employee
  • 1591 Views
  • 0 replies
  • 2 kudos

STM32H750VB uart errors

Hi,I have a problem using UART7 on STM32H750VB. It is configured by STM32CubeMx to receive and transmit with DMA with a baud rate of 115200 but all the data that arrive from the external device cause FRAME or NOISE errors.I checked with my oscillosco...

ENove.1 by Associate II
  • 2526 Views
  • 6 replies
  • 0 kudos

Resolved! Why can't I see SPI4 clk and MOSI signals in Transmit Mode Only Master STM32H743ZI2 with an oscilloscope ?

Hello, I am trying to use SPI programmable amplifier MCP6S21 from TI with my STM32H743ZI2 nucleo board but nothing seems to happen. When I try to observe the signals from CLK and MOSI pins, there is nothing (even when it is supposed to be transmittin...

M.CHN by Associate III
  • 1817 Views
  • 3 replies
  • 0 kudos

STM32CubeMX 5.6.0 (latest) Generated BLE projects cannot build!

Hi, I updated everything to the latest CubeMX and packages. When I generate BLE code now (just a simple P2P Server) the build fails because of multiplye defined symbols. Anyone a soluition?compiling app_ble.c...../Src/app_ble.c(224): warning: #1296-D...

F F by Associate II
  • 3137 Views
  • 7 replies
  • 0 kudos

STM32 HAL_Delay doesn't work properly

Hello,I'm in the process of learning the STM32 MCU. I have the STM32F4DISCOVERYBOARD with a STM32F407VGT on it.At first I tried the simple LED blink tutorial and noticed that the LED will light up, but won't blink.I did some more attempts and figured...

0693W000001sF0SQAU.png 0693W000001sEzyQAE.png 0693W000001sF0XQAU.png 0693W000001sF3qQAE.png
DFile.1 by Associate II
  • 3002 Views
  • 5 replies
  • 0 kudos

STM32cubeMx project to ac6 dsp 0xF THUMBmode

Hi,I am a new bee to STM ...tried generating the code to get the UART up for STM32L476 series discovery board...but could not compile the code in ac6 compiler as this gives following errorError: selected processor does not support `isb 0xF' in Thumb ...

RShiv.1 by Senior
  • 3711 Views
  • 12 replies
  • 0 kudos

Resolved! Using FreeRTOS with TrustZone in STM32CubeIDE - STM32L562

I have a development kit for the STM32L562, I'm trying to create a blinky-script that will use FreeRTOS to blink a led in the secure-world and the non-secure world simultaneously.Steps to reproduce:Install STM32CubeIDE 1.3.0New STM32 ProjectLook for ...

FHumb.1 by Associate II
  • 5308 Views
  • 10 replies
  • 0 kudos

Bug in CubeMX v 5.6.1 when selecting DMA for ADC1/2 and BDMA for ADC3 for STM32H753IITx? Is there a fix or have I done something wrong?

Generated code in main.c looks like this and lacks function name for the second block./**  * Enable DMA controller clock */static void MX_BDMA_Init(void) { /* DMA controller clock enable */ __HAL_RCC_BDMA_CLK_ENABLE(); /* DMA interrupt init */ /* BD...

DGrön.1 by Associate II
  • 1530 Views
  • 3 replies
  • 0 kudos