2023-12-04 12:46 PM
Hi,
I have project for STM32F405 created manually. Project is using fixed GCC 4.92014q4.
After updating STM32CubeIDE to version 1.14.0 i got warnings shown below.
Compiler option "Cyclomatic Complexity" is disabled.
File "subdir.mk" contains this rule:
# Each subdirectory must supply rules for building sources it contributes
Src/%.o Src/%.su Src/%.cyclo: ../Src/%.c Src/subdir.mk
How to remove this warnings?
2025-06-18 3:52 AM
Try downgrade make.exe to older version. I overwrite make.exe in CubeIDE v1.18 (used with GCC v14.2) with version from v1.13 (GNU Make 4.2.1_st_20200221-0903_longpath) and problem with "pattern recipe" disperse. Make directory: STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.make.XXX\tools\bin.
2026-02-19 1:27 AM
I installed STM32CubeIDE V2.0.0 on my M4 Mac laptop and tried to compile a project from my old Mac Intel laptop but it couldn't find the compiler:
/bin/sh: arm-none-eabi-gcc: command not found
I assumed I needed to install the compiler and the search AI's gave me a brew install recipe to do so. Once I installed the compiler and tried to compile, it recognized the compiler but I got a ton of messages about "cycolomatic complexity" and "stack usage" options not supported. I wiped all traces of the compiler, IDE and special directories again using AI recipes. But after once again following the steps carefully, I ended up at the same no pass.
I backed up a step and removed the compiler to take me back to the missing compiler message. I created a makefile.init to be run by make and placed a 'printenv' command in it to let me see the local environment that it was trying to compile in.
The PATH variable is the issue. It lists a path to a different version of the compiler which is not installed. The compiler is in a different directory
To fix it, I added a symbolic link for the directory that it was looking for to the one that exists:
ln -s com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.macos64_1.0.100.202509120712 com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.13.3.rel1.macos64_1.0.0.202411102158And now it works!
The wrong path must come from somewhere - perhaps there is an internal setting that could be changed.
I am running the same version of the IDE on a different Mac Intel laptop and there is no problem. The correct compiler directory exists. My guess would be that the M4 install uses a directory for a different version of the compiler and internally when it creates the compile environment, it used the Intel compiler path. Perhaps the new compiler didn't get into the release? I don't know but very obscure bug. Thanks to these forum posts, I was able to reason it out and get a simple fix.
2026-02-27 1:58 AM
Now that my Intel Mac has updated, it has the same problem of not having the right path to the compiler. The above fix worked again. It is applied in the directory:
/Applications/STM32CubeIDE.app/Contents/Eclipse/plugins