2023-11-23 12:56 AM
Hello
the brand new 1.14.0 has the same issue like the older one.
an unnecessary file is opened after the 2nd debug session.
It's annoying that STM can't get this solved.
padawan
Solved! Go to Solution.
2023-11-23 07:54 AM
Hello @padawan
Thanks for reporting.
Actually, after checking internally, this is a known issue that have been already reported to dev team and tracked with the internal ticket 162500 and this will be fixed asap.
Thx
Souhaib
2023-11-23 01:24 AM
2023-11-23 01:34 AM
Thanks for this,
i followed the thread but it will not work.
if i open the debug session it open the .s fille
padawan
2023-11-23 07:54 AM
Hello @padawan
Thanks for reporting.
Actually, after checking internally, this is a known issue that have been already reported to dev team and tracked with the internal ticket 162500 and this will be fixed asap.
Thx
Souhaib
2024-02-01 01:21 AM
@Souhaib MAZHOUD Any chance you can give us some feedback on the progress of internal ticket 162500
2024-02-09 05:12 AM
3 months passed. but sadly still didn't fixed...
2024-04-16 07:25 AM
Almost 4 years of jumping to random files after pressing the Run button. What's another 4 months...
2024-04-16 11:53 PM
@Souhaib,
Opening an internal ticket is not a solution, it is poor.
An "asap" that takes 4 years is certainly not a solution.
padawan
2024-06-16 03:25 AM
Same issue, version: Version: 1.15.1, Win11, new CubeIDE installation. Problem started at the very first project (I started to learn programming MCUs recently) .
2024-09-12 03:44 PM
After 4 years is still not resolved...
What is the status? Can you please provide an update and an ETA?
Thank you