PWM Timer Issue in stm32go70rbt6 controller
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-27 7:10 AM
Hi All,
I'm working on stm32g070rbt6 controller, for vending project.
For some requirement implemented PWM timer(i.e. TIM1 & Channel 2) to run the dc motor(i.e. 24V). based on the input from keypad.
PWM implemented with soft start from 0 to 1800 which is 90% duty cycle and ARR value is 2000. @500Hz frequency
Currently facing an issue with motor, it will work fine for some duration after some time motor will run continuously and it will not stop at all and no other function will work. It feels like hang and this scenario will happen only for this particular timer and channel.
We tracked all kind of fault cases and error cases via UART log no where it is hitting.
Note:- There is only one interrupt, which is 4ms(i.e. TIM7) for data updating to LCD.
Kindly give suggestions on this issue to figure out the exact issue.
Regards,
Nikhil
- Labels:
-
STM32CubeIDE
-
STM32CubeMX
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-27 7:32 AM
Can you connect with a debugger and do a memory read of TIM1? Also could check the GPIO settings to see if something in code took over that particular GPIO.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-06-27 10:12 PM
We couldn't be able to check with debugger for long time because the issue will not come frequently and cross verified the pin nowhere it is configured except for timer (Tim1).