2024-01-18 12:03 PM
Hello
I open project in CubeIDE and in hardware/software configuration select Software Packs Components Selector, in TouchGFX option for latest version selected and blue button with Install label next to it , with yellow man icon , but it is disabled and I can’t select it. selector with options in last row also disabled . Currently on this computer TouchGFX v 4.21.0 installed , project was copied from another computer and implemented with TouchGFX v 4.21.3. How could I fix this. Thank you
Solved! Go to Solution.
2024-01-18 11:34 PM
Hello @rBlr
The yellow Icon means that you should Login to download the software package. Then, you can download the package and select the Graphics application.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-01-18 11:34 PM
Hello @rBlr
The yellow Icon means that you should Login to download the software package. Then, you can download the package and select the Graphics application.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.