cancel
Showing results for 
Search instead for 
Did you mean: 

Error while start debugging: could not determine GDB version using command: arm-none-eabi-gdb

PaulB
Associate II

Get this error when trying to start debug. Debug starts fine after I restart the IDE.

version of STM32CubeIDE is 1.13.1, Windows7.

1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Evangelist III

Note that your Windows version is not supported by CubeIDE. link

View solution in original post

5 REPLIES 5
Semer CHERNI
ST Employee

Hello @PaulB 

First let me thank you for posting.

Could you send the debug log which could be in the console or generated under: Debug Configuration>Debugger>Log to file

SemerCHERNI_0-1698763589280.png

BR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

I'm using Segger J-LINK. There is no such option as Log to file

 

up

Hello Semer,

please, check out my answer.

Pavel A.
Evangelist III

Note that your Windows version is not supported by CubeIDE. link