STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1477 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 571 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Projects not building after update

Hi, today I updated CubeIDE to version 1.3.1 and my working projects and also newly generated projects won't build. I'm getting 114 error messeges of this type: "Error: selected processor does not support `dsb ' in Thumb mode". Also in project settin...

ANiko.2 by Associate
  • 1155 Views
  • 1 replies
  • 0 kudos

Build multiple binary files in 1 project

Hello there :I want to build multiple bin files with specific address and length in CubeIDE/Eclipse,for example , I have my linker file like :MEMORY:{ SYSTEM_BIN(wr) :ORIGIN = 0x8008800 ,LENGTH = 8K PCU_BIN(wr) :ORIGIN = 0x800A800 ,LENGTH = ...

WYang.2 by Associate
  • 2373 Views
  • 3 replies
  • 1 kudos

Resolved! DMA IRQ Handler is called twice for ADC

Hi,I am using 3 ADC modules triggered with TIM3 to start in the same time.I read the result in the DMAx_Channely_IRQHandler function and for debug only I do a toggle in a GPIO.I have 3 DMAx_Channely_IRQHandler functions , one for each ADC with DMA an...

DKuro.1 by Associate III
  • 1928 Views
  • 2 replies
  • 0 kudos

HAL libraries and LL libraries version & download links.

Hello,I am comparing the STM32Cube IDE (the suggested from ST) and OpenSTM32 IDE HAL system organization and I have a few questions about it:Is there a way to know the HAL libraries version ? Actually I don't see this parameter.Is it possible to down...

simo zz by Senior II
  • 2931 Views
  • 1 replies
  • 1 kudos

Resolved! Create an assembly project

Hi, For education purpose, I'm trying to create, compile, load and debug assembly projects with STM32Cube. Unfortunately, there are no built in options to do it. I noticed that I can erase on an existing project the main.c and create a main.s instead...

SToru.1 by Associate
  • 4260 Views
  • 2 replies
  • 0 kudos

STM32Cube 1.3.0 - Error: bind failed. Error = 98, exit

Hi,I am using STM32CubeIDE 1.3.0 on Linux Debian, and when I try to flash the MCU using the Run Button, GDB fails with error "bind failed. Error = 98, exit" (it seems that the IDE is trying to open an busy connection).Concretely the log from console ...

simo zz by Senior II
  • 1366 Views
  • 1 replies
  • 1 kudos

bug report: STM32F302CBT6 failed to compile

Hi, This particular MCU is not fully populate in project generator, the result when trying to create a project is incomplete project that can't compile. I worked-around by selecting a different MCU, but as migrating between MCU is not supported, I am...

BVauc.1 by Associate II
  • 1571 Views
  • 3 replies
  • 0 kudos