STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1427 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Hello, I am trying to program STM32F103 MCU barebone. I attached it to LQFP 48 adaptor and made connections to Vcc, GND and clock as in Bluepill module. Using STMCUBE IDE For controlling RGB LED, the code has been debugged and unable to flash.

Error: Info : clock speed 1800 kHzError: init mode failed (unable to connect to the target)in procedure 'init' in procedure 'ocd_bouncer'I set high freq clock as ceramic resonator (used 8Mhz clock chipset) and with STLINK V2 debugger. Please let me k...

NU.2 by Associate
  • 1872 Views
  • 3 replies
  • 0 kudos

Error while flashing GPIO_EXTI program on STM32F746ZG board

Not able to flash GPIO_EXTI program on STM32F746ZG board using CubeIDE toolSource code : https://github.com/STMicroelectronics/STM32CubeF7/tree/master/Projects/STM32F746ZG-Nucleo/Examples/GPIO/GPIO_EXTIEnvironment : Ubuntu 18.04.4 LTSCube IDE : STM32...

DV.3 by Associate
  • 2794 Views
  • 1 replies
  • 0 kudos

Problem Testing System Timer on STM32CubeIDE

Hello,I am trying to step through the How To guide for bringing up a board in the TouchGFX documentation. During "Step 2. CPU Running" I ran into an issue with the step that tests the system timer. I was able to execute the first test regarding the c...

Sayali by Associate II
  • 1461 Views
  • 2 replies
  • 0 kudos

CubeIDE + Linux + stm32vldiscovery pipeline doesn't work

Hi All!I'm trying to flash my first project to stm32vldiscovery using CubeIDE under Linux (ubuntu 18.04). I tried different debug configuration, but I didn't meet success. I saw different errors such as "Target unknown error 27" or just "Failed to st...

STM32L476RG: RTC shows delay in time

Hi all,I am working with FreeRTOS on STM32L476RG and I'm new to this. I am using stm32cubeIDE for project development. I am printing the date and time in the putty and the time format is hours: minutes: seconds: subseconds. When I start running the p...

Resolved! Fail to open the debugger after upgrade CubeIDE to V1.3.1

After I upgrade the CubeIDE to the latest version I'm not able any more to debug a project that before the upgrade was working fine.My current CubeIDE version is Version: 1.3.1 Build: 6291_20200406_0752 (UTC)Muy cube programmer is V2.4.0And the error...