STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1443 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Float value gives hard fault in STMCubeIDE

Dear All:I want to use the FPU module in STM32F407,But how can i use it in STM32Cubeide?and i use UCOS_III.If I define a floating point data,when i use this data,it will be case HardFault.add the libopen the FPUdefine __VFP_FP__but in SystemInit FPU ...

0693W000001sIopQAE.png 0693W000001sIpJQAU.png 0693W000001sIpTQAU.png 0693W000001sIr0QAE.png
赵静.1 by Associate
  • 2111 Views
  • 1 replies
  • 0 kudos

#define example file on CubeIDE

Does someone could point out where can I find one CubeIDE file full of complex "#define" examples? When I use more sofisticated #define into Cube IDE I receive tons of "error" messages (I mean "error message" not warnings). But into other compilers t...

JSILV.2 by Senior
  • 6201 Views
  • 10 replies
  • 0 kudos

can anybody help ? make: *** [makefile:94: touch.elf] Error 1

I am getting this error it has something to do with FLash memory I guessc:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:...

MNapi by Senior III
  • 1149 Views
  • 2 replies
  • 0 kudos

STM32F746IGT with DAC enabled

Hi,I am using Stm32CubeIDE v1.3.1 with my custom STM32F746IG board and touchGFX enabled (working properly with 800x480 paralel LCD). I have tried to play with DAC channels (Channel1-2). I can not get it work through the examples with DMA enabled or w...

istepne by Associate III
  • 1244 Views
  • 1 replies
  • 0 kudos
AKuma.10 by Associate
  • 1250 Views
  • 2 replies
  • 0 kudos

View Stack pointer in Stm32Cube IDE

Hi,I have just started with STM32 and got some basic programs running. I wanted to understand stack pointer and program counter.Please help me how do i view Stack pointer in CubeIDE during Debug mode.IDE version 1.3.0

A memory hole! what does this mean?

Dear experts,I'm debugging a program on STM32H753 in Atollic TS 9.3 and see something weird.It looks like unreadable hole in D1 RAM from 0x24013880 to 0x24013BAFIs this artifact of the Atollic's debugger, or???The chip runs at 400 MHz

0693W000001s4H3QAI.jpg 0693W000001s4HNQAY.jpg
Pavel A. by Super User
  • 1593 Views
  • 3 replies
  • 0 kudos

How to obtain the dwarf2 file to simulate with proteus isis

Hi all, I'm trying to simulate a project made in STM32Cube IDE for an STM32F103C6 in proteus ISIS but for debug purposes labcenter's people says that I need the .elf file and the dwarf2 file (both of them in the same folder), then I' found that GCC f...

VRami.1 by Associate III
  • 2060 Views
  • 2 replies
  • 1 kudos