STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1406 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 556 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32CUBE IDE FreeRTOS cmsis_os.h:461:67: warning: ISO C++ forbids converting a string constant to 'char*'

When freeRTOS header cmsis_os.h is used in *.cpp file, it generates compiler warningISO C++ forbids converting a string constant to 'char*'.Proposed fix:Change line 326 of cmsis_os.h from:typedef struct os_thread_def { char                  *name;   ...

MBel.1 by Associate
  • 1245 Views
  • 0 replies
  • 2 kudos

Not able to flush the firmware in STM32F413RH custom board

Hello,I could use DISCO-F413ZH (STM32F413ZH MCU) dev board to test some of the sensors. After successfully testing with dev board, I made custom board using STM32F413RH MCU. When I connect the custom board to computer, it detects as STM32 bootloader....

VKart.1 by Associate
  • 4103 Views
  • 2 replies
  • 0 kudos

Float value gives hard fault in STMCubeIDE

Dear All:I want to use the FPU module in STM32F407,But how can i use it in STM32Cubeide?and i use UCOS_III.If I define a floating point data,when i use this data,it will be case HardFault.add the libopen the FPUdefine __VFP_FP__but in SystemInit FPU ...

0693W000001sIopQAE.png 0693W000001sIpJQAU.png 0693W000001sIpTQAU.png 0693W000001sIr0QAE.png
赵静.1 by Associate
  • 2091 Views
  • 1 replies
  • 0 kudos

#define example file on CubeIDE

Does someone could point out where can I find one CubeIDE file full of complex "#define" examples? When I use more sofisticated #define into Cube IDE I receive tons of "error" messages (I mean "error message" not warnings). But into other compilers t...

JSILV.2 by Senior
  • 6141 Views
  • 10 replies
  • 0 kudos

can anybody help ? make: *** [makefile:94: touch.elf] Error 1

I am getting this error it has something to do with FLash memory I guessc:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe:...

MNapi by Senior III
  • 1125 Views
  • 2 replies
  • 0 kudos