STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1556 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 589 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

"EXTIX_IRQHandler" not found.

I tried this tutorial on NUCLEO-L412RB-P, it was said "The HAL_EXTIX_IRQHandler and EXTIX_IRQHandler are inside stm32l4xx_it.c file.", I haven't find "EXTIX_IRQHandler" there, is it in somewhere else, or it was needed for L412RB-P?(the tutorial based...

MQi.1 by Senior II
  • 2259 Views
  • 4 replies
  • 1 kudos

hrlp! - debug as says (none applicable)

I'm trying to run a simple blink sketch using a F031K6 nucleo board. I'm following the steps here - https://www.youtube.com/watch?v=hyZS2p1tW-g and when i get to the part where I go to 'debug as' I can't because it says 'none applicable'. I have the ...

deep_rune by Associate III
  • 2902 Views
  • 9 replies
  • 0 kudos

Timer for 3 s interrupts after 8 s

Hi ! I am currently using STM32 Nucleo-L073RZThe problem is that I've set it to 3 s but it executes after 8 s. In a different application it finished exactly after 3 s. I just don't understand what went wrong. The code looks like that : What main has...

Xenon02_0-1702571070276.png Xenon02_1-1702571087813.png Xenon02_2-1702571096793.png
Xenon02 by Senior
  • 3519 Views
  • 7 replies
  • 2 kudos

STM32CubeIDE hangs when opening MX /.ioc view

starting the IDE is like rolling the dice every day : will it start and run perfect - or not ?this happens about once in 100 starts, then it hangs in the splash window and you cannot do anything more.seems to be a "well known" thing, there is some wo...

AScha3_0-1701072615096.png
AScha.3 by Super User
  • 3125 Views
  • 4 replies
  • 0 kudos

STM32CubeIDE can't connect (No device found on target)

Have been using STM32CubeIDE with several processors and different Nucleo boards with successAcquired a Nucleo-U575ZI and when I try to download code I get:STMicroelectronics ST-LINK GDB server. Version 6.0.0Copyright (c) 2021, STMicroelectronics. Al...

Hcorw.1 by Associate II
  • 2338 Views
  • 3 replies
  • 0 kudos

NUCLEO-F103RB: No device found on target.

Hello,For the past two days I have started experimenting with STM32F0 and STM32F1 Nucleo Boards and the STM32CubeIDE, so I am not that experienced yet. Everything went fine but suddenly, I was not able anymore to program my NUCLEO-F103RB board. It th...

WBach by Associate II
  • 1851 Views
  • 1 replies
  • 0 kudos

Resolved! Hard Fault on function start - but cannot debug

I have a problem, but dont know, how to solve...when this function ( mp3dec_decode_frame(..) ) is used, get hard fault. ok, but cannot debug , because no step into function is possible, hard fault is always next step.Now the prerequisites : this func...

AScha3_0-1701984656178.png AScha3_1-1701984719271.png AScha3_2-1701984805304.png AScha3_3-1701984845368.png
AScha.3 by Super User
  • 18951 Views
  • 34 replies
  • 2 kudos

DCACHE on STM32U599

Hi!I'm configuring the STM32U599VJT with CubeMX enabling DCACHE1 and 2, as well as ICACHE. Code is generated without error, but functions like SCB_CleanDCache_by_Addr() are not enabled as the definitions in stm32u599xx.h do not include __ICACHE_PRESE...

paolog by Senior
  • 3528 Views
  • 4 replies
  • 1 kudos

lwIP deadlock with a twist

Setup:MCU: STM32F429PHY: DP83848 (MII)Advertised Mode: 10BASE-T, Half/Full-Duplex 100BASE-TX, Hal/Full-DuplexOS: CMSIS-RTOSv2CubeMX: Yes Just wanted to start of with mentioning that i've read and tried the fixes  provided by @Piranha. I've tried the ...

XD by Associate III
  • 3635 Views
  • 4 replies
  • 0 kudos