cancel
Showing results for 
Search instead for 
Did you mean: 

Clangd IntelliSense issues: plugin-generated --query-driver incomplete for C++, and multi-lib-config triggers errors

lconlcong
Associate II

I am using the STM32Cube VS Code extension (Preview) with the official ST-ARM-CLANG and clangd for code completion. Just ran into two issues:

1. Incomplete --query-driver config breaks C++ IntelliSense

The extension adds

--query-driver=${env:CUBE_BUNDLE_PATH}/st-arm-clang/19.1.6+st.8/bin/starm-clang.exe

to settings.json by default, but this is not enough for C++ files.
Unless you also add

--query-driver=${env:CUBE_BUNDLE_PATH}/st-arm-clang/19.1.6+st.8/bin/starm-clang++.exe

C++ IntelliSense will be broken (red squiggles, no symbols, etc).
Same issue for GCC toolchain: you need both gcc and g++ in the driver list.

2. --multi-lib-config triggers errors in clangd

If you enable --multi-lib-config, clangd just starts throwing errors about missing headers and stuff, even though the project still compiles fine.
Is this a known issue? Anyone have a workaround?

By the way, is there any official way to download the standalone ST Arm Clang toolchain (without the VSCode extension)?
It would be super useful for CI/CD or automation, similar to how STM32CubeCLT was distributed before.

Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions
lconlcong
Associate II

To be honest, stm32cube-clangd's only job seems to be unconditionally reporting errors whenever it sees st-arm-clang options—even though these are perfectly valid for STM32. If you want real code completion, just use the regular clangd extension instead—at least it doesn't freak out over STM32's own toolchain.

View solution in original post

6 REPLIES 6
FluxPower42
Associate III

 

Same here.
I work with a VSCode workspace, and these settings are stored in the 'ProjectName.code-workspace' file.
Unfortunately, VSCode deletes the following entry every time the workspace is opened:
"--query-driver=${env:CUBE_BUNDLE_PATH}/st-arm-clang/19.1.6+st.8/bin/starm-clang++.exe".

An entry with a wildcard is replaced after opening the workspace.
"--query-driver=${env:CUBE_BUNDLE_PATH}/st-arm-clang/19.1.6+st.8/bin/starm-clang*".
=> no solution

You can see this behaviour in the attached video.

  • Timecode 0:00
    A STM32CubeMx project with Cpp sources was compiled before the video is recorded with the
    '--query-driver=${env:CUBE_BUNDLE_PATH}/st-arm-clang/19.1.6+st.8/bin/starm-clang++.exe' entry without any issues.
  • Timecode 0:12 
    VS Code is closed.
  • Timecode 0:17 
    VS Code reopens by double-clicking the STM32Firmware.code-workspace file.
  • Timecode 0:29
    The entry is removed automatically.
  • Timecode 0:40
    CMake: Detele Cache an Reconfigure
  • Timecode 0:46
    CMake: Clean Rebuild
  • Timecode 0:57
    Still "No Problems" - but wait...
  • Timecode 1:02After opening a .cpp file, some problems appear, such as 'Unknown Compiler', and so on.

Please provide a solution for this. Thanks!

 

lconlcong
Associate II

To be honest, stm32cube-clangd's only job seems to be unconditionally reporting errors whenever it sees st-arm-clang options—even though these are perfectly valid for STM32. If you want real code completion, just use the regular clangd extension instead—at least it doesn't freak out over STM32's own toolchain.

Except STM clangd extension sounds to be original one clone (per readme comment) just hacking it revisiting way to get clangd utility itself. Not sure moving back to original is helpful here. 

What is your expérience so far doing it ?

Mainline clangd works better. It fully recognizes all st-arm-clang options and does not show any errors. Also, the settings are not messed up by STM32Cube plugin. I recommend just using official clangd.

FluxPower42
Associate III
vincent_grenet
ST Employee

Please be aware that stm32cube-ide-build-cmake-1.40.1.vsix has been released to address C++ concerns.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.