STM32CubeIDE for Visual Studio Code (MCUs)

Ask questions on the STM32CubeIDE for Visual Studio Code extension. Find answers on a variety of topics, including build issues, debug functionalities, CMake project integration, and feature requests for CubeCLT installation.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Debug Issues: Exception has occurred.

Hi, When I insert a breakpoint or pause the debugger, the debugger first stops at a point where there was probably an ISR, showing the error message in the figure below, and I need to press F5 again so that the degugger goes to the breakpoint that I...

0693W00000aJH2kQAG.png
Asantos by Senior
  • 2234 Views
  • 1 replies
  • 0 kudos

Resolved! How to install for windows 10?

I have (I believe) installed all the prerequisites and added the paths to STM32CubeMX and STMCUFinder. However I cannot use the extension as the commands are not available.​If I try to run the command via the command palette, I get a "command not f...

0693W00000aJMiCQAW.jpg 0693W00000aJMibQAG.jpg
Macdog by Associate III
  • 2399 Views
  • 1 replies
  • 0 kudos