cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 VS Code Extension (No compiler found in cache file)

Legacy member
Not applicable

I am trying to get the STM32 VS Code Extension working on my macOS (Ventura 13.2.1). I have installed STM32CubeCLT and STM32CubeMX. I can compile my project successfully using the build command command. However when I press on the debug icon on the bottom toolbar, I get an error saying that "No compiler found in cache file Source Make Tools (Extension)" (See attached screenshot). I have examined the build/debug/build/CMakeCache.txt file and everything looks ok at first glance. Any insight or solutions as to what is going on would be welcomed.

10 REPLIES 10
MM1
Associate II

Hey there,

I am running into the same issue. has it been resolved yet?

Greetings Marcus