2025-09-24 8:38 AM - edited 2025-09-24 8:59 AM
bitbake st-image-weston -c populate_sdk This works without the populate-sdk option
with the SDK an python error occurs
I can't find a way to get around this by cleanstate or clean glibc.
Attached the log.
Then did:
bitbake -ccleansstate glibc-locale
bitbake glibc-locale
which went fine (see attachment)
but then the build failed again with the same error
Solved! Go to Solution.
2025-09-25 7:25 PM - edited 2025-09-25 7:26 PM
Deleted the repo and started the build all over again. Now the SDK and Weston image are all successfully build. it takes about 160GB. This after about 4 to 5 errors that could be recovered from with cleanall. Attached the result. There are a few warnings. Question remains, how to recover from failures as in this post that could not be recovered from ? Perhaps ST can dedicate a wiki about such Yocto issues (assuming engineered have encountered these as well (they may have a knowledge base).
2025-09-25 7:25 PM - edited 2025-09-25 7:26 PM
Deleted the repo and started the build all over again. Now the SDK and Weston image are all successfully build. it takes about 160GB. This after about 4 to 5 errors that could be recovered from with cleanall. Attached the result. There are a few warnings. Question remains, how to recover from failures as in this post that could not be recovered from ? Perhaps ST can dedicate a wiki about such Yocto issues (assuming engineered have encountered these as well (they may have a knowledge base).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.