cancel
Showing results for 
Search instead for 
Did you mean: 

How to properly add include paths in STM32CubeIDE CMake Project?

parmi93
Associate II

I'm working on an STM32 project using STM32CubeIDE with CMake as the build system. I need to add custom include paths for my own header files.

I tried to include my_folder from C/C++ General -> Paths and Symbols -> Includes, but it doesn't work.

parmi93_0-1764339432467.png

Note that under C/C++ Build -> Settings there is no settings to include anything, which are available only when working with STM32CubeMX/STM32CubeIDE Project

parmi93_1-1764339652146.png parmi93_2-1764339662730.png

 

 

2 REPLIES 2
Andrew Neil
Super User

Right-click a folder in the Project Explorer:

AndrewNeil_0-1764340250791.png

I would hope that would do things "properly" ...

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.

The Add/remove include path... option is not clickable...

parmi93_0-1764341834003.png