cancel
Showing results for 
Search instead for 
Did you mean: 

How to install OpenSTLinux plugin for STM32CubeIDE 2.0.0 MPU projects

Aimen1
ST Employee

If STM32CubeIDE v2.0.0 is installed from scratch and if the imported project in STM32CubeIDE v2.0.0 is a project generated with STM32CubeMX v6.16, then it is not possible to install the OpenSTLinux plugin, consequently, it is not possible neither to import OSTL Projects: Linux, Optee, TF-A, U-Boot.

In order to work around this, the following steps are recommended:

  • Install STM32CubeIDE 1.19.0
  • Install OpenSTLinux plugin v6.1.0 in STM32CubeIDE 1.19.0
  • Import the projects concerned (Linux, Optee, TF-A, U-Boot)
  • Help > Check for updates > select STM32CubeIDE 2.0.0 > Next > Finish
  • Then restart the STM32CubeIDE.

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
0 REPLIES 0