cancel
Showing results for 
Search instead for 
Did you mean: 

Issue with terminal output at putty with simple Helloworld program using Nucleo-L522ZE-Q.

raitaimoorali
Associate II

 

 

 

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2023 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ ADC_HandleTypeDef hadc1; UART_HandleTypeDef hlpuart1; UART_HandleTypeDef huart2; RTC_HandleTypeDef hrtc; PCD_HandleTypeDef hpcd_USB_FS; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); static void MX_ADC1_Init(void); static void MX_LPUART1_UART_Init(void); static void MX_RTC_Init(void); static void MX_UCPD1_Init(void); static void MX_USB_PCD_Init(void); static void MX_USART2_UART_Init(void); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_ADC1_Init(); MX_LPUART1_UART_Init(); MX_RTC_Init(); MX_UCPD1_Init(); MX_USB_PCD_Init(); MX_USART2_UART_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ char buffer[]="Hello World\r"; HAL_Delay(100); HAL_UART_Transmit(&huart2, (unsigned char *)&buffer, 6, sizeof(buffer)); HAL_Delay(1000); HAL_GPIO_TogglePin (GPIOC, GPIO_PIN_7); } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE0) != HAL_OK) { Error_Handler(); } /** Configure LSE Drive Capability */ HAL_PWR_EnableBkUpAccess(); __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSE |RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.HSI48State = RCC_HSI48_ON; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = RCC_MSICALIBRATION_DEFAULT; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 55; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK) { Error_Handler(); } } /** * @brief ADC1 Initialization Function * @PAram None * @retval None */ static void MX_ADC1_Init(void) { /* USER CODE BEGIN ADC1_Init 0 */ /* USER CODE END ADC1_Init 0 */ ADC_MultiModeTypeDef multimode = {0}; ADC_ChannelConfTypeDef sConfig = {0}; /* USER CODE BEGIN ADC1_Init 1 */ /* USER CODE END ADC1_Init 1 */ /** Common config */ hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc1.Init.Resolution = ADC_RESOLUTION_12B; hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc1.Init.ScanConvMode = ADC_SCAN_DISABLE; hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV; hadc1.Init.LowPowerAutoWait = DISABLE; hadc1.Init.ContinuousConvMode = DISABLE; hadc1.Init.NbrOfConversion = 1; hadc1.Init.DiscontinuousConvMode = DISABLE; hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START; hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc1.Init.DMAContinuousRequests = DISABLE; hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED; hadc1.Init.OversamplingMode = DISABLE; if (HAL_ADC_Init(&hadc1) != HAL_OK) { Error_Handler(); } /** Configure the ADC multi-mode */ multimode.Mode = ADC_MODE_INDEPENDENT; if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK) { Error_Handler(); } /** Configure Regular Channel */ sConfig.Channel = ADC_CHANNEL_3; sConfig.Rank = ADC_REGULAR_RANK_1; sConfig.SamplingTime = ADC_SAMPLETIME_2CYCLES_5; sConfig.SingleDiff = ADC_SINGLE_ENDED; sConfig.OffsetNumber = ADC_OFFSET_NONE; sConfig.Offset = 0; if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN ADC1_Init 2 */ /* USER CODE END ADC1_Init 2 */ } /** * @brief LPUART1 Initialization Function * @PAram None * @retval None */ static void MX_LPUART1_UART_Init(void) { /* USER CODE BEGIN LPUART1_Init 0 */ /* USER CODE END LPUART1_Init 0 */ /* USER CODE BEGIN LPUART1_Init 1 */ /* USER CODE END LPUART1_Init 1 */ hlpuart1.Instance = LPUART1; hlpuart1.Init.BaudRate = 209700; hlpuart1.Init.WordLength = UART_WORDLENGTH_8B; hlpuart1.Init.StopBits = UART_STOPBITS_1; hlpuart1.Init.Parity = UART_PARITY_NONE; hlpuart1.Init.Mode = UART_MODE_TX_RX; hlpuart1.Init.HwFlowCtl = UART_HWCONTROL_NONE; hlpuart1.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; hlpuart1.Init.ClockPrescaler = UART_PRESCALER_DIV1; hlpuart1.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; hlpuart1.FifoMode = UART_FIFOMODE_DISABLE; if (HAL_UART_Init(&hlpuart1) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&hlpuart1, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&hlpuart1, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&hlpuart1) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN LPUART1_Init 2 */ /* USER CODE END LPUART1_Init 2 */ } /** * @brief USART2 Initialization Function * @PAram None * @retval None */ static void MX_USART2_UART_Init(void) { /* USER CODE BEGIN USART2_Init 0 */ /* USER CODE END USART2_Init 0 */ /* USER CODE BEGIN USART2_Init 1 */ /* USER CODE END USART2_Init 1 */ huart2.Instance = USART2; huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONE_BIT_SAMPLE_DISABLE; huart2.Init.ClockPrescaler = UART_PRESCALER_DIV1; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetTxFifoThreshold(&huart2, UART_TXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_SetRxFifoThreshold(&huart2, UART_RXFIFO_THRESHOLD_1_8) != HAL_OK) { Error_Handler(); } if (HAL_UARTEx_DisableFifoMode(&huart2) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USART2_Init 2 */ /* USER CODE END USART2_Init 2 */ } /** * @brief RTC Initialization Function * @PAram None * @retval None */ static void MX_RTC_Init(void) { /* USER CODE BEGIN RTC_Init 0 */ /* USER CODE END RTC_Init 0 */ RTC_PrivilegeStateTypeDef privilegeState = {0}; /* USER CODE BEGIN RTC_Init 1 */ /* USER CODE END RTC_Init 1 */ /** Initialize RTC Only */ hrtc.Instance = RTC; hrtc.Init.HourFormat = RTC_HOURFORMAT_24; hrtc.Init.AsynchPrediv = 127; hrtc.Init.SynchPrediv = 255; hrtc.Init.OutPut = RTC_OUTPUT_DISABLE; hrtc.Init.OutPutRemap = RTC_OUTPUT_REMAP_NONE; hrtc.Init.OutPutPolarity = RTC_OUTPUT_POLARITY_HIGH; hrtc.Init.OutPutType = RTC_OUTPUT_TYPE_OPENDRAIN; hrtc.Init.OutPutPullUp = RTC_OUTPUT_PULLUP_NONE; if (HAL_RTC_Init(&hrtc) != HAL_OK) { Error_Handler(); } privilegeState.rtcPrivilegeFull = RTC_PRIVILEGE_FULL_NO; privilegeState.backupRegisterPrivZone = RTC_PRIVILEGE_BKUP_ZONE_NONE; privilegeState.backupRegisterStartZone2 = RTC_BKP_DR0; privilegeState.backupRegisterStartZone3 = RTC_BKP_DR0; if (HAL_RTCEx_PrivilegeModeSet(&hrtc, &privilegeState) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN RTC_Init 2 */ /* USER CODE END RTC_Init 2 */ } /** * @brief UCPD1 Initialization Function * @PAram None * @retval None */ static void MX_UCPD1_Init(void) { /* USER CODE BEGIN UCPD1_Init 0 */ /* USER CODE END UCPD1_Init 0 */ LL_GPIO_InitTypeDef GPIO_InitStruct = {0}; /* Peripheral clock enable */ LL_APB1_GRP2_EnableClock(LL_APB1_GRP2_PERIPH_UCPD1); LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOB); LL_AHB2_GRP1_EnableClock(LL_AHB2_GRP1_PERIPH_GPIOA); /**UCPD1 GPIO Configuration PB15 ------> UCPD1_CC2 PA15 (JTDI) ------> UCPD1_CC1 */ GPIO_InitStruct.Pin = LL_GPIO_PIN_15; GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; LL_GPIO_Init(GPIOB, &GPIO_InitStruct); GPIO_InitStruct.Pin = LL_GPIO_PIN_15; GPIO_InitStruct.Mode = LL_GPIO_MODE_ANALOG; GPIO_InitStruct.Pull = LL_GPIO_PULL_NO; LL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* USER CODE BEGIN UCPD1_Init 1 */ /* USER CODE END UCPD1_Init 1 */ /* USER CODE BEGIN UCPD1_Init 2 */ /* USER CODE END UCPD1_Init 2 */ } /** * @brief USB Initialization Function * @PAram None * @retval None */ static void MX_USB_PCD_Init(void) { /* USER CODE BEGIN USB_Init 0 */ /* USER CODE END USB_Init 0 */ /* USER CODE BEGIN USB_Init 1 */ /* USER CODE END USB_Init 1 */ hpcd_USB_FS.Instance = USB; hpcd_USB_FS.Init.dev_endpoints = 8; hpcd_USB_FS.Init.speed = PCD_SPEED_FULL; hpcd_USB_FS.Init.phy_itface = PCD_PHY_EMBEDDED; hpcd_USB_FS.Init.Sof_enable = DISABLE; hpcd_USB_FS.Init.low_power_enable = DISABLE; hpcd_USB_FS.Init.lpm_enable = DISABLE; hpcd_USB_FS.Init.battery_charging_enable = DISABLE; if (HAL_PCD_Init(&hpcd_USB_FS) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN USB_Init 2 */ /* USER CODE END USB_Init 2 */ } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); __HAL_RCC_GPIOA_CLK_ENABLE(); __HAL_RCC_GPIOB_CLK_ENABLE(); __HAL_RCC_GPIOG_CLK_ENABLE(); HAL_PWREx_EnableVddIO2(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOA, GPIO_PIN_5|LED_RED_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED_GREEN_GPIO_Port, LED_GREEN_Pin, GPIO_PIN_RESET); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(GPIOB, UCPD_DBN_Pin|LED_BLUE_Pin, GPIO_PIN_RESET); /*Configure GPIO pins : PA5 LED_RED_Pin */ GPIO_InitStruct.Pin = GPIO_PIN_5|LED_RED_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /*Configure GPIO pin : UCPD_FLT_Pin */ GPIO_InitStruct.Pin = UCPD_FLT_Pin; GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(UCPD_FLT_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pin : LED_GREEN_Pin */ GPIO_InitStruct.Pin = LED_GREEN_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED_GREEN_GPIO_Port, &GPIO_InitStruct); /*Configure GPIO pins : UCPD_DBN_Pin LED_BLUE_Pin */ GPIO_InitStruct.Pin = UCPD_DBN_Pin|LED_BLUE_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

 

 

raitaimoorali_0-1693514054813.png

raitaimoorali_1-1693514108650.png

Led is getting toggled but not getting anything at serial output. Please help. Thanks

 

12 REPLIES 12

>>I am not sure did i miss something? 

The schematic and the user manual? You don't link to the tutorial, so no idea here if it refers to this board, or something else. The ST-LINK VCP has specific wired connectivity to a UART on the STM32L5, LPUART1 is the primary, and you'd have to change a lot of solder bridges to accommodate USART3 on PD8/PD9

To use USART2 you need to wire the pins up to a USB-to-CMOS Serial adapter from SiLabs, FTDI, et al.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Here's the Manual and Schematic if you missed, or couldn't find, them

https://www.st.com/resource/en/user_manual/um2581-stm32l5-nucleo144-board-mb1361-stmicroelectronics.pdf

https://www.st.com/resource/en/schematic_pack/mb1361-l552zeq-c02_schematic.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thanks.