STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USART3 platform_get_irq faild

Hy i am using the usart3 from the STM32MP157A-DK1. i orientated myself on the USART driver (https://elixir.bootlin.com/linux/latest/source/drivers/tty/serial/stm32-usart.c).butwhen i want to initialize theport I get following error code “Rs453Network...

SAman.1 by Associate III
  • 4378 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157: Booting the M4 out of the A7 context fails when the RSVD mux function is used

Hi CommunityIn the DT the TIM1, TIM4 and SPI4 are assigned to the M4 and in the pinmux the RSVD is set (DT attached). Booting A7 generates no ERROR during Kernel boot. If the M4 is started from the A7 context the following ERROR Messages occurs for a...

KWyss.1 by Associate II
  • 1926 Views
  • 1 replies
  • 0 kudos

Hi, I recently buy a STM32MP157F-DK2 kit and I would want to connect some RS232 devices (one or two), can you suggest me some RPI Hats or Arduino add on shields compatibles with the card ? Thanks

I don't want to use a usb to serial adapter because I need the 9th bit available in the UART and this converters are not generally compatible with that

HSant.1 by Associate II
  • 820 Views
  • 2 replies
  • 0 kudos