2024-10-20 11:51 PM
Hello I got succeed wlan0 connect to my phone just yesterday
Ping 8.8.8.8 was worked and etc ok(without booting make 1m30s timeout)
But today it is not working at all with just doing same before
After enable and start wireless config with
systemctl enable wpa_supplicant@wlan0.service
systemctl restart systemd-networkd.service
systemctl restart wpa_supplicant@wlan0.service
Or wpa_supplicant -B -iwlan0 -c /etc/wpa_supplicant/wpa_supplicant.conf
The error log is repeating on my console...
What should i check?
Thanks
2024-10-21 5:49 AM
Hi @SKim.1761
please share more background on the issue
which board are you using ?
STM32MP157F-DK2 ? else ?
Which OpenSTLinux ecosystem are you using ?
Latest is v5.1.0: https://wiki.st.com/stm32mpu/wiki/STM32_MPU_ecosystem_release_note
Maybe share full console log.
Regards.
2024-11-12 9:18 PM - edited 2024-11-12 9:19 PM
I am trying stm32mp157f-dk2
I cannot answer about echosystem well,, just I can say just I am using starter package image
Anyway that problem is on smartphone's hotspot wifi only
I tried in home's wifi router it worked