Questions about STM32MP157C-DK2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-25 12:35 AM
Hello! I have just discovered that kit I would like to use to develop a new testing system within the company where I am working. However, I have some questions about it:
- What kind of additional card could we use to apply 24V to the board's input (I have to use the output signal of the inductive sensor currently used)?
- Does it exist a card which can directly get 24V as an input voltage (or is it always 5V or 3.3V)?
- How many analogical, numerical and On/Off I/O does the kit's board have?
- Could we use some software like Matlab to analyse the output signals of that card?
I truly thank you in advance for your answers!
Sincerely,
Labels:
- Labels:
-
STM32MP15 Lines
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-03-09 1:16 AM
Hello @NAnt.3
In case you haven’t seen yet, some information can be found in the User Manual for the board on st.com
- Input voltage is only 5 V / 3 A USB Type-C™power supply input
- Available IO’s can be seen in the
◦ GPIO expansion connector (Raspberry Pi® shields capability)
◦ Arduino™ Uno V3 expansion connectors
Best Regards
JM