cancel
Showing results for 
Search instead for 
Did you mean: 

Patch/help to make TFA updatable within the ST FWU (firmware update) procedure

maxim-senec
Associate II

Hi everyone,

we applied the ST FWU reference solution on our own platform based on the STM32MP157F.
The solution was taken and adapted from the ST Yocto layer meta-st-ota (https://github.com/PRG-MPU-CUST/meta-st-ota).

We have a few questions to clarify the default behavior:

  1. What is the default behavior in the early boot stage 

    Do we understand correctly that fsbl1 and fsbl2 are intended to contain identical TF-A images for fail-safe purposes, and that the ROM looks for the first valid FSBL (starting from fsbl1) and loads it?

  2. Rollback behavior at ROM / TF-A layer

    Is it correct that there is no FWU rollback concept implemented in ROM / TF-A itself?
    I.e. fsbl1 is not treated as part of a bank like [fip-a, bootfs-a, rootfs-a], but instead the two FSBL slots are only there to allow a second try to load the same TF-A version from fsbl2 if fsbl1 fails?

  3. Updating TF-A over-the-air

    If we decide to update TF-A via OTA (with RAUC and the ST FWU solution), do we understand correctly that:

    • TF-A needs to be included in the bundle, and

    • the new TF-A image must be written to both fsbl1 and fsbl2 to keep the ROM fail-safe behavior?

  4. Guidance for making TF-A updateable

    Are there any ST documents, examples or patches you can point us to that describe the recommended way to make TF-A updateable in an FWU / RAUC setup on STM32MP1?


Thank you very much for any help!

 

1 REPLY 1
Christophe Guibout
ST Employee

Hello @maxim-senec,

 

1. Yes : 1-2 suffix is to duplicate image content for redundancy purpose. 

2. Yes. ROM code has an anti-rollback mechanism, but not linked with FWU. fsbl1 and fsbl2 are not supposed to be updated.

3. Yes and Yes. Nevertheless, in case of failure of the new image, you can't be sure to come back on the previous image because fsbl* have been updated.

4. No. The point is : why updating TF-A BL2 ?

 

BR,

Christophe

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.