STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

stm32mp135 boot stuck

NOTICE: CPU: STM32MP135F Rev.YNOTICE: Model: STMicroelectronics STM32MP135F-DK STM32CubeMX board - openstlinux-6.1-yocto-mickledore-mp1-v23.06.21NOTICE: BL2: v2.8-stm32mp1-r1.0(release):custom()NOTICE: BL2: Built : 15:38:01, Jul 2 2025NOTICE: BL2: Bo...

Resolved! STM32MP257F-DK GStreamer problem

Hello,I'm using Buildroot environment with the STM32MP257F-DK board. I'm testing GStreamer with a simple pipeline:gst-launch-1.0 videotestsrc ! autovideosinkWhen I first run it there is no problem. The test video shows fine on the HDMI monitor. But w...

Ronte.1 by Associate III
  • 1836 Views
  • 6 replies
  • 0 kudos