STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Support RTL8211E-VB-CG in STM32MP157

We designed our own board and use RTL8211E instead of RTL8211EG-VB-CG. We are unable to get the PHY device to respond although we copy the same circuit from the MB1262. The MAC is working but the communication to Realtek PHY seems to be a problem. ...

aman.32 by Associate II
  • 5034 Views
  • 6 replies
  • 0 kudos

I'm trying to find a solution to a problem using vision with ANN/CNN - STM32Cube.AI or X-LINUX-AI-CV or FP-AI-VISION1 or X-CUBE-AI

I'm trying to find a solution to a problem using vision, I discovered the 'MPU' line with the STM32MP157C-DK2 but while investigating I cannot find CSI input or even a camera input. While I enjoy playing with USB based cameras it is 2019 and everyone...

KevinA by Senior
  • 2061 Views
  • 5 replies
  • 0 kudos

opengl no wayland

Is it possible to use opengl without wayland?the /vendor/lib libraries have dependency to libwaylandand as far as i am aware these libraries are binary only.are there other versions of the libraries that can work with fb, without x or wayland?otherwi...