STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Create a 32b parallel bus

Hello, I am working on the stm32mp157-dk1. I would like to create a 32bits parallel bus on cortex A7, at a frequency greater than 20Mhz but when I do a test on a pin I get a max frequency of 120khz, which is too low. I think this is the wrong program...

FJouf.1 by Associate II
  • 3839 Views
  • 6 replies
  • 0 kudos

STM32MP157A-DK1 UART3 kernel module

Hy wanted to make a kernel Module and i wanted to know whats the best way to acces the uart from Kernel Space.So far i enabled the UART in the device try and now i am able to send data. But now i know since the uart us in userspace i cant access it f...

SAman.1 by Associate III
  • 1606 Views
  • 2 replies
  • 0 kudos

Resolved! STM32MP1 ethernet error message

I have a question about the Starter Package.When I start STM32MP157x-EV1 (+en.FLASH-stm32mp1-openstlinux-5-4-dunfell-mp1-20-11-12), I get the following logroot@stm32mp1:~# dmesg | grep ether[   1.642061] stm32-dwmac 5800a000.ethernet: PTP uses main c...

rmaki.1 by Associate II
  • 3995 Views
  • 4 replies
  • 0 kudos

Linux running on A7 corrupted when FreeRTOS with virtual uart application running on CM4 freeze. How to fix this in Linux 5.4.31?

We have an virtual uart FreeRTOS application running on CM4, it captures SPI data and sends to A7 through virtual uart. Sometimes, the FreeRTOS application freezed, A7 can not read the data through /dev/ttyRPMSG0 again, at the same thime, Linux 5.4....

SunnyGeGe by Associate III
  • 848 Views
  • 0 replies
  • 0 kudos

Unable to build logic analyzer example

I'm trying to build the large buffer exchange example but have been unsuccessful so far. I have the distribution installed and have no problem building the default package but when I try to build with the logic analyzer I get repo failures and compi...

WCast.1 by Associate II
  • 4941 Views
  • 10 replies
  • 0 kudos