STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Unable to install AI packages

Reference: https://wiki.st.com/stm32mpu/wiki/X-LINUX-AI_OpenSTLinux_Expansion_Package#Configure_the_AI_OpenSTLinux_package_repositoryNote that I am still using v2.0.0.I used to be able to do the following execution on my board, but it is not working ...

JYune by Associate II
  • 1946 Views
  • 2 replies
  • 0 kudos

QSPI Clock Question

Hi,Is there a way to set the QSPI clock on the MP157 to be free running while also using the QSPI? The programming manual mentions that free running mode will prevent the QSPI from being usable.I am working on a project to interface the MP157 to an F...

hjups22 by Associate II
  • 2426 Views
  • 4 replies
  • 0 kudos

Resolved! STM32MP157A-DK1 �?�미지 업로딩 중 오류

STM32MP157A-DK1보드�? �?�미지 다운로딩 중 오류가 �?�?니다.​https://wiki.st.com/stm32mpu/index.php/STM32MP15_Discovery_kits_-_Starter_Package여기 �?료를 참고로 진행하다 오류가 �?겨 진행�?� 못하는 �?태입니다.보드를 구입 후 받았�?� 때 SD카드(기존�? ST�?서 제공해 주는 리눅스가 깔려 있�?� SD 카드)�? 다운로딩�?� 진행했습니다.​현재 H...

0693W000008G6tpQAC.png
SBae.4 by Associate II
  • 2118 Views
  • 4 replies
  • 0 kudos