STM32 MPUs Products and hardware related

Ask questions and find answers on STM32 microprocessors, including hardware, power, DRAM, flashing, interfacing, device tree, and peripherals.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How do I fix "undefined reference to `OPENAMP_create_endpoint'" within the OpenAmp source.

I've added OPENAMP through the middleware after enableing the IPCC interrupts, but now I'm getting the following error and an error in the actual OPENAMP source that's included!/opt/st/stm32cubeide_1.8.0/plugins/com.st.stm32cube.ide.mcu.externaltools...

msche.1 by Associate III
  • 2015 Views
  • 1 replies
  • 0 kudos

Resolved! Time of erase after a tamper

Hi all,I am using MPU ref. STM32MP153F, do you say me what is the time that elapsed between a tamper is detected and the backup resister are finishing erased?And the backup SRAM?Thank you in advance

FAlca.1 by Associate II
  • 1805 Views
  • 1 replies
  • 0 kudos

Resolved! STM32MP157 Errata 2.3.8, "eMMC boot Timeout too short", causes problems with available eMMCs.

The STM32MP157 demands a maximum time of 10 ms from reset command to boot partition data. According to JEDEC No 84-B51 the maximum time from reset command to the first data is up to 1 second (tBD):All data sheets of eMMCs that I found specify their b...

0693W00000KcGd5QAF.png
SigiBue by Associate
  • 2315 Views
  • 3 replies
  • 0 kudos

Resolved! STM32MP157C with MII PHY not working

I am using a KSZ9021GN PHY in MII mode. Due to supply chain issues we had to resort to this PHY. (Cube MX says I can't use GMII mode). I am experiencing this apparently common issue: [ 15.650981] dwmac4_dma_reset err [ 15.652849] stm32-dwmac 580...

BillR by Senior
  • 3773 Views
  • 3 replies
  • 0 kudos