2023-06-06 03:15 AM
Following the tutorial on How to customize the Linux kernel I made steps as below:
FILESEXTRAPATHS:prepend := "${THISDIR}:${THISDIR}/${PN}:"
KERNEL_CONFIG_FRAGMENTS:append = "${WORKDIR}/fragments/${LINUX_VERSION}/fragment-custom.config"
SRC_URI:append = " file://${LINUX_VERSION}/fragment-custom.config;subdir=fragments "
It seems that the kernel configuration wasn't applied at all, is there something that I'm doing wrong?
Without the FILEXTRAPATHS line, the file couldn't be found, yocto didn't look into my-layer at all.
Solved! Go to Solution.
2023-06-07 03:33 AM
Well, if the file /tmp-glibc/work/stm32mp13_rt-ostl-linux-gnueabi/linux-stm32mp/5.15.67.rt49-stm32mp-r1-r0/build/.config is equivalent with the final configuration, then changing the layer priority didn't help at all.
2023-06-07 04:42 AM
OK I continue to test so.
By the way, I confirm that you need the
FILESEXTRAPATHS:prepend := "${THISDIR}/${PN}:"
in your bbappend file, only way to ensure that the path is in the research path of Yocto.
2023-06-07 04:45 AM
Good to know, I think this should be included in your tutorial How to customize the Linux kernel: https://wiki.st.com/stm32mpu/wiki/How_to_customize_the_Linux_kernel
2023-06-07 04:52 AM
Yes, good remark, we will add it for sure.
By the way, I tested your layer on a standard weston image provided by ST.
It seems that the .config file is well modified in the build repository of Linux.
I give you my steps:
Put the attach layer under layers/meta-st
Then bitbake-layers add-layer ../layers/meta-st/meta-my-layer
Then bitbake linux-stm32mp
Finally, when I check <..>/build-openstlinuxweston-stm32mp15-disco/tmp-glibc/work/stm32mp15_disco-ostl-linux-gnueabi/.config it seems that your fragment is well taken into account.
Can you also double check from your side ?
Kind regards,
Erwan.
PS: I needed to adapt the layer.conf for my environment which is ST native delivery.
2023-06-07 05:19 AM
I'll try that tomorrow, as today my work day is about to finish. There's one thing which I forgot to mention and may be quite important - instead of the disco image/distro/machine, I used the image with the RT patch, which means that meta-st-x-linux-rt layer with the stm32mp13-rt MACHINE were involved as well. Could it be so that the build behaves differently for the RT variant?
The other two things I get constantly are a WARNING message and a NOTE message as below, sorry for not mentioning about these before:
NOTE: ../layers/meta-st/meta-st-openstlinux/recipes-st/images/st-image-resize-initrd.bb: ENABLE_PARTITIONS_IMAGE not enabled2
WARNING: ../layers/meta-st/meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_5.15.bb:do_compile is tainted from a forced run
I'm not sure what "tainted" from a forced run means, this are messages run after bitbake st-image-weston.
Okay, thank you for your help, as mentioned already, I'll test your advice tomorrow.
2023-06-07 05:44 AM
OK thanx for the additional information.
Let me know tomorrow when you will have done your tests.
Kind regards,
Erwan.
2023-06-08 12:52 AM
I just followed your steps and reproduced the fixes, indeed I can already see the config in tmp-glibc/work/stm32mp13_disco-ostl-linux-gnueabi/linux-stm32mp/5.15.67-stm32mp-r2-r0/build/.config. However I do have a few questions.
Beforehand I was building the st-image-weston, your advice says differently. Is there any benefit to using the linux-stm32mp image instead of st-image-weston, what's the difference between them? Actually, is that even an image? The contents of meta-st-stm32mp/recipes-kernel/linux/linux-stm32mp_5.15.bb do look like an image recipe, but it doesn't live in an image directory as it's usually the case. However there's plenty of images in meta-st-stm32mp layer, but in the meta-st-stm32mp/recipes-st/images directory. So I'm a bit confused, can you explain?
Also, how does that linux-stm32mp differ from the st-image-weston?
2023-06-08 12:57 AM
Hello @Antoni Jankowski ,
Sure, this is just to win some time 🙂
Indeed, I just build the Linux kernel recipe when I do this manipulation, because it saves me some time instead of compiling all the weston image. I just wanted to check and give you a quick answer.
Of course, building only the Linux recipe does not create you your final image. But when you compile st-image-weston it will also compile linux-stm32mp recipe.
So, in conclusion, you should be able to see the same .config generated when you do a bitbake st-image-weston (if not, there is an issue in the Yocto compilation).
Kind regards,
Erwan.
2023-06-08 01:03 AM
Okay, I'll check with the full st-image-weston and get back to you. There's a lot of checking to be happening today :(
2023-06-08 01:05 AM
Sure, let me know.
If you still does not see it at the very end, maybe make a try with putting your fragment in the x-linux-rt recipe to see if it changes something (because I do not have it on my baseline).
Kind regards,
Erwan.