cancel
Showing results for 
Search instead for 
Did you mean: 

Excluding gpio from Linux

Bennny
Associate III

Hello.

Is there any way to exclude some GPIOs from Linux, when I control them from M4 core and I don't want to give an ability to control them from Linux apps? I would like to exclude e.g. PG12. I tried this, which should be exactly for such use:

&gpiog {
   gpio-reserved-ranges = <12 1>; /* Reserve PG12 for M4 */
};

 
But it doesn't help, still the GPIO is listed and possible to control under Linux.

We use OpenSTLinux custom Yocto build with kernel 5.15.67

Thanks

4 REPLIES 4
OlivierK
ST Employee

Hi @Bennny,

 

Have you tried m4_reserved_gpios ?

 

m4_reserved_gpios {

    compatible = "st,m4-reserved-gpios";

    gpio-reserved-ranges = <...>;

};

 

Bear in mind that OpenSTLinux 5.15 is not anymore supported, if possible please point to the latest OSTL release.

 

Regards,

Olivier


In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Bennny
Associate III

Thanks for the reply.
I tried to find any info about the m4-reserved-gpios, but I didn't find any definition of it in docs, source code nor google.
Also the gpio-reserved-ranges = <...>; is in such case counted from GPIOA 0 (so PG12 is 108)?

Bennny
Associate III

Could you please provide the description/documentation of the m4_reserved_gpios and the gpio-reserved-ranges calculation?

Bennny
Associate III

Are these responses AI? Because it's the same thing which ChatGPT gave me before I wrote here on the forum...