Skip to main content
Associate II
July 1, 2024
Solved

ecosystem v5.1.0 - Cannot fetch meta-st-openstlinux

  • July 1, 2024
  • 2 replies
  • 1532 views

I am trying to update my distribution (dated ecosystem v.5.0.0) to ecosystem v.5.1.0 ,

As repoted in

https://wiki.st.com/stm32mpu/wiki/STM32MP1_Distribution_Package#Building_the_OpenSTLinux_distribution

I ran :

` repo init -u https://github.com/STMicroelectronics/oe-manifest.git -b refs/tags/openstlinux-6.1-yocto-mickledore-mpu-v24.06.26`

followed by `repo sync`, but I get the following error:

error: Cannot fetch meta-st-openstlinux from https://github.com/STMicroelectronics/meta-st-openstlinux
Fetching: 100% (1/1), done in 3m14.826s
fatal: failed to unpack tree object HEAD
error.GitError: Cannot checkout meta-st-openstlinux: Cannot initialize work tree for meta-st-openstlinux
error: Cannot checkout meta-st-openstlinux
Checking out: 85% (6/7), done in 1.078s
error: Unable to fully sync the tree
error: Downloading network changes failed.
error: Checking out local projects failed.
Failing repos:
layers/meta-st/meta-st-openstlinux
Try re-running with "-j1 --fail-fast" to exit at the first error.
================================================================================
Repo command failed due to the following `SyncError` errors:
GitCommandError: 'fetch --quiet --progress OpenSTLinux --prune --recurse-submodules=no --tags +refs/heads/*:refs/remotes/OpenSTLinux/* +refs/tags/*:refs/tags/*' on meta-st-openstlinux failed
stdout: remote: Enumerating objects: 3384, done.
GitCommandError: 'fetch --quiet --progress OpenSTLinux --prune --recurse-submodules=no --tags +refs/heads/*:refs/remotes/OpenSTLinux/* +refs/tags/*:refs/tags/*' on meta-st-openstlinux failed
stdout: remote: Enumerating objects: 3384, done.
Cannot initialize work tree for meta-st-openstlinux

 

I also tried to git clone that repo (https://github.com/STMicroelectronics/meta-st-openstlinux.git)  but it still gives me error.

Thank you for fixing it.

$ git clone https://github.com/STMicroelectronics/meta-st-openstlinux.git my-meta-st-openstlinux
Cloning into 'my-meta-st-openstlinux'...
remote: Enumerating objects: 3384, done.
remote: Counting objects: 100% (1290/1290), done.
remote: Compressing objects: 100% (775/775), done.
error: RPC failed; curl 92 HTTP/2 stream 0 was not closed cleanly: CANCEL (err 8)
error: 3876 bytes of body are still expected
fetch-pack: unexpected disconnect while reading sideband packet
fatal: early EOF
fatal: fetch-pack: invalid index-pack output
This topic has been closed for replies.
Best answer by luaiza

Hello, thank you for answering.

I beleive the issue is on my side (even though I haven't detected it yet) - sorry.

2 replies

Olivier GALLIEN
ST Technical Moderator
July 1, 2024

Hi @luaiza ,

Thanks for your interest in this new release.

Note that official announcement and wiki update might be done by this Wednesday .. you are an early adopter :smiling_face_with_smiling_eyes:

Anyway, just checked my end and didn't get any problem. 

Worth to check if any network issue at your end and retry. 

Olivier 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
luaizaAuthorBest answer
Associate II
July 3, 2024

Hello, thank you for answering.

I beleive the issue is on my side (even though I haven't detected it yet) - sorry.