cancel
Showing results for 
Search instead for 
Did you mean: 

Device serial number

allard
Senior

Simple question:

If i'm right the serial number returned by cat /sys/firmware/devicetree/base/serial-number is the UID from BSEC. Where is the code responsible for setting this value? I've seen the function get_board_serial in u-boot but it doesnt seem to be implement for the stm32mp1 board.

2 REPLIES 2
PatrickF
ST Employee

Hi @allard ,

not sure it answer your question.

The 96-bits UID is set in factory (i.e. fused inside OTP), readable thru BSEC. It cannot be altered and it is guaranteed to be unique within a STM32MP serie.

Regards.

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.

This I understand.

What i'm trying to do is replace the function that reads the UID with a function that reads my own serial number programmed into the OTP.

I've looked for the function that does the reading but i've not found it. I'm using the distribution package. So my question is: where is the read implemented, so I can make a .patch to patch this to read my own serial number.