2025-02-27 9:26 AM
Hello all,
I am trying to find the SVD file for STM32WBA55CG.
I was looking at https://github.com/stm32-rs/stm32-rs/tree/master since I want to use svd2rust to generate a pac that I can use to implement a bare-metal function in the microcontroller. However, in the repo, svd files are located in the vendor folder and they are .zip files.
I managed to locate an SVD file downloading the STM32CubeIDE and searching for it in the installation path but there are errors when using svd2rust, which is why I wanted to use the repo mentioned above, and ideally, including it.
Thanks
2025-02-27 11:33 AM
Hello @elopezpe and Welcome to the ST Community.
The SVD file of the STM32WBA55CG is not yet available. But it will be shared on this link When available.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.