2025-02-26 8:39 PM
I am trying to make a prototype from a perf-board and a QFN48 adapter using STM32WL55CC MCU based on the wiring in the pics below. I want to connect to the MCU using SWD via an STlink attached to a Nucleo board. I already removed the 2 jumpers on CN2 and made the following connection shown below to CN4 and the MCU. However when i try to connect using the ST-Link utility I am getting the following error. BTW I just started learning embed development and just want to connect via SWD for now.
Connection Details:
VDD_TARGET(PIN1 on CN4)=>3.3V supply from PIN16 CN7 on the nucleo board
SWCLK(PIN2 on CN4)=>PIN 42 on STM32Wl55CC
GND(PIN3 on CN4)=>ground pad on STM32Wl55CC
SWDIO(PIN4 on CN4)=>PIN 36 on STM32Wl55CC
NRST(PIN5 on CN4)=>NRST on TM32Wl55CC
VDD for the MCU is supply from 3.3V CN7 PIN16 of the nucleo board
2025-02-26 8:54 PM
What about all the other power connections? RF and SMPS? These do not seem optional even in LDO mode.
https://www.st.com/resource/en/datasheet/stm32wl55cc.pdf
Consider buying a known good board for development. Having decoupling caps so far from the chip is not ideal.
https://www.st.com/en/evaluation-tools/nucleo-wl55jc.html
2025-02-27 10:19 AM
Thanks for the feedback. Based on the reference design documentation (see pic) I came to the conclusion that the RF and SMPS are not needed for just connecting via SWD for programming. Also the I am using the MB1789_LP-LowBand_LowPower reference design as a guide. I did not use a Nucleo-Wl55 development board because I eventually will need to develop my own board if I am to deploy anything serious and I want to delve deeper into the hardware development side.