cancel
Showing results for 
Search instead for 
Did you mean: 

STM32WB55 freezing when returned from STOP2 after RTC wakeup

fo
Associate II

Hello,

I modified the BLE Beacon example to send 5 beacon packets and then enter into the STOP2 mode. It is possible to wake-up and resend 5 packets when a button is activated. However, when the time is set, the MCU wakes-up, and freeze.

The function UTIL_LPM_EnterLowPower() is used for entering low-power, and HAL_RTCEx_SetWakeUpTimer_IT() is used for setting the wake-up time. a few seconds are used as wake-up time. The wake-up is only verified by monitoring the current consumption increased from few µA to approx. 2.5mA after the time is elapsed. Beside that turning on one of the LEDs has been implemented in the RTC wake-up interrupt routine, and one just after the __WFI without it's being triggered.

It has not been possible to debug, as the debug does not return until the execution is paused, and when it's paused the PC points on the next line of the __WFI instruction.

Do you have any ideas of what the reason can be, or any suggestion on debugging?

Best regards,
Fatih

 

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @fo 

Could you please try to use a HW timer for the walke up instead of using the RTC. I think there is not an accuracy problem since the LPM is based on the RTC. So, i think this should help you.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
STTwo-32
ST Employee

Hello @fo 

Could you please try to use a HW timer for the walke up instead of using the RTC. I think there is not an accuracy problem since the LPM is based on the RTC. So, i think this should help you.

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

fo
Associate II

Hello,

I managed to solve the issue, and for those that face the same challenge, here is the explanation. It seems that the RTC of the HW timer has higher priority than the others. The device wakes up at the expected time, however as all the HW timers are stopped, the device does nothing. When a HW timer is used as @STTwo-32 suggests, all seems to work.