cancel
Showing results for 
Search instead for 
Did you mean: 

STM32 Boards with WiFi connectivity

fafik25
Associate

Hello,

Is there is any board delivered by STM32 with WiFi capabilities?

BR

1 ACCEPTED SOLUTION

Accepted Solutions
Issamos
Lead III

Hello @fafik25 

There is not an ST MCU delivered with embedded WiFi capability. But, if you are looking for an evaluation board that include an external WiFi module (not an ST module) you may find some such as the The STM32H7B3I-DK. You can also use any MCU with the ST67W611M WiFi module from ST.

Best Regards.

II 

View solution in original post

2 REPLIES 2
Issamos
Lead III

Hello @fafik25 

There is not an ST MCU delivered with embedded WiFi capability. But, if you are looking for an evaluation board that include an external WiFi module (not an ST module) you may find some such as the The STM32H7B3I-DK. You can also use any MCU with the ST67W611M WiFi module from ST.

Best Regards.

II 

mƎALLEm
ST Employee

Hello,

I can suggest the B-L475E-IOT01A, it features plenty of wireless connectivity interfaces including Wi-Fi (802.11 b/g/n )

mALLEm_0-1762421711310.png

 

 

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.