2025-09-11 7:38 AM - edited 2025-09-15 12:52 AM
Hi, I'm planning to use a STM32WB5MMG for a custom board. For this application, I need to measure the frequencies and the duty cycles of three different PWM signals. I know that there is the PWM Input mode of some TIM. However, I verify that there are only two timers with this function. How can I overcome this limitation? Can I use Input Capture direct/indirect mode of the timers?
Thanks.
Matteo