2024-09-18 11:15 AM
Hello, I am using the NucleoWL55 for transmitting and receiving the data. I am able to transmit and receive the data in HEX, and when I observed in SDR# using RTL SDR I observed the burst data. I want to know if the NucleoWL55 can transmit the CW data or not?,,
Please, help
2024-10-01 02:11 AM
Hello @D_Sajan
Yes, it is possible to transmit Continuous Wave (CW) data using the STM32WL.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.