cancel
Showing results for 
Search instead for 
Did you mean: 

Can't run Zephyr BLE peripheral example on Nucleo-n657x0-q & x-nucleo-wb05kn1

BKaiwalya
Associate II

Hello, 

I am using Zephyr v4.3.99 and want to build and run the BLE peripheral example from samples\bluetooth\peripheral for the following targets:

 

I carried out the following steps:

  • flashed the "~\x-cube-wb05n\Utilities\BLE_Transparent_Mode_STM32WB05_controller_only\UART\BLE_TransparentMode_UART_with_Updater_C_O.hex" .hex file from  X-CUBE-WB05NV2.0.0 / 20-March-2025  package
  • Built the peripheral example using
west build -b nucleo_n657x0_q --shield x_nucleo_wb05kn1_uart samples\bluetooth\peripheral

 

The project builds successfully but I can not see the default advertisement, what could be wrong? @Sebastien DENOUAL 

0 REPLIES 0