STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB55RC ZIGBEE Stack Address

We are trying to load the stm32wb5x_Zigbee_FFD_fw.bin on STM32WB55RC, but the address table in the release note show as 0x00 for FFD stack and STMCube Programmer gives error as bad address.What is the actual address for Zigbee stack for 256K Flash de...

YSN by Senior
  • 1854 Views
  • 2 replies
  • 0 kudos

Resolved! Can Phy be set to 2M when connected to a Windows App?

Hello,I was just wondering whether it was possible to form a 2M PHY connection with a Windows BLE App?I have developed firmware for my STM32WB nucleo board, along with a C#.NET Windows application to connect with it.I am trying to maximise throughput...

OCatt.1 by Associate II
  • 3621 Views
  • 6 replies
  • 0 kudos

Resolved! SUBGHZ_PHY middleware: why is it necessary to configure the UART? Is it possible to transmit a LoRa message without using the UART pins?

I am trying to transmit a single int using LoRa and the SUBGHZ_PHY middleware. However, I am unsure as to why UART has to be configured under 'Platform Settings', and how I can setup the STM project for this purpose. I am using STM32CubeIDE, and a Nu...

Rvan .8 by Associate II
  • 1604 Views
  • 2 replies
  • 2 kudos

Resolved! AN2606 Rev 50 - Documentation Error

In Table 150 ("STM32WLE5xx/55xx configuration in system memory boot mode") on page 380.In the section "USART2 bootloader", "USART1" must be replaced by " USART2".Thank you.JL

JLemi by Associate III
  • 1288 Views
  • 1 replies
  • 0 kudos

Stm32wb55 board drawing high current

Hi,I have a custom PCB using the STM32WB55 running at 32MHZ. For some reason my board is drawing high current ~40mA. I’m trying to rule out anything I may have missed connection wise on the WB. Would anyone have any ideas if this high current draw is...

kcire L. by Associate III
  • 572 Views
  • 0 replies
  • 0 kudos

New design based on STM32WB55CGU6 Microcontroller

I have a new design based on STM32WB55CGU6 Microcontroller. I wanted to use the MLPF-WB55-1E03 IPD Device for Maching Network. However, the device seems to be out of stock world wide.Can I replace it with MLPF-WB55-02E3?

GKhar.2 by Associate
  • 954 Views
  • 1 replies
  • 0 kudos