STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB55RGV6(can't find ble device) I just change from gpio_raising_it to gpio falling_it(PC11). My led still can toggle, just can't find ble device.

I just change from gpio_raising_it to gpio falling_it(PC11). When I use raising edge interruption, all is well. When I use falling edge interruption, my led still can toggle, just can't find ble device. So I think my board can work, it's just a blue...

Lep by Senior
  • 648 Views
  • 0 replies
  • 0 kudos

I used STM32WB55RGV6 to make a board (BLE server), the USB dongle is used as (BLE client), and then the USB dongle is output to the computer through the serial port.

I used STM32WB55RGV6 to make a board (BLE server), the USB dongle is used as (BLE client), and then the USB dongle is output to the computer through the serial port. I need to further organize and categorize this data, and then display it as a real-t...

Lep by Senior
  • 676 Views
  • 0 replies
  • 0 kudos

STM32WLE5(RAK3172) - Why do we need to initialize and de-initialize the ADC function again and again for every read, whether this method is effective?

I'm currently working on stm32WLE5(RAK3172) for that module, and I'm using SDK 1.0.0V  1) In that LoRaWAN stack for battery reading implementation, we are noticing that the ADC initialization & de-initialization happening every time.My question is, w...

0693W00000Svy7DQAR.png 0693W00000Svy78QAB.png

Resolved! STM32WB Zigbee: How to set the PowerSource to Battery and report Battery Voltage and Remaining percentage

Hello, I'm trying to make a Zigbee application for a battery powered device (currently using the ZHA integration on Home Assistant) and I am having trouble to set the attribute for a battery power source, (it seems to be stuck on the default of Mains...

0693W00000Su1QjQAJ.jpg
earlish by Associate II
  • 3191 Views
  • 3 replies
  • 1 kudos

Resolved! STM32WB55 - ACI_HAL_TONE_START command rf channel resolution

Hi everyone,I use STM32WB55 with the BLE stack 13.0 (full version) and want to test the RF. In the an5270 document, I noticed the ACI_HAL_TONE_START command and it is allowed to change the rf channel from 2.402 to 2.480 GHz with 2 MHz resolution. How...

serhat by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos

Resolved! aci_gap_create_connection() returns 0x3a

I have a STM32WB that serves as the master and four other as the slaves.As the slaves may sometimes go offline, the master will periodically tries to connect with them (say, every 10 seconds). Between two connection attempts, the master allows the co...

HLin.3 by Associate II
  • 1932 Views
  • 2 replies
  • 0 kudos

stm32wb5x_BLE_Stack_full_fw.bin (used resources)

Dear all,I am looking for a reference document listing the resources (timers, RAM, GPIOs, bus clocks etc) that are used by the Bluetooth stack provided byST (stm32wb5x_BLE_Stack_full_fw.bin).Any idea where I can find a complete documentation?Thanks a...